Part Number: PCM2900
Hello,
I want to USB interface to send a specific voltage value to the PC.
The specific voltage is just DC Voltage.(0~3.3V range)
So, I need to A/D and USB transceiver.
Among the single chip, I found the PCM2900C.
Is it possible to do the above mentioned using the PCM2900C?
If it is impossible , Please let me know if there are any other alternatives or different ways.