Other Parts Discussed in Thread: PCM1860
I am trying to implement BT audio loop back test with the following schematic using PCM1860 and PCM5122.
PCM1860 is configured in hardwire mode with fs = 44.1kHz, I2s mode, channel#1 activated. PCM5122 is also configured in hardwire mode with clock signals (BCK and LRCK) in slave mode, I2S mode, etc.
Once VINL1 and VINR1 of PCM1860 are supplied with 250Hz 1Vpp sinusoidal wave, I am expecting similar sinusoidal waves at OUTL and OUTR of PCm5122. But I got nothing on OUTL and OUTR. Attached please find captured DIN, BCK and WCK at PCM5122 input side. Measurements results: f_WCK = 44.1kHz and f_BCK=64*44.1kHz = 2.817MHz.
what am I missing?
Since PCM5122 has slave clock BCK and WCK as inputs. Does it still need a SCK clock?
Thanks,