Hello
I am currently working on an application where the area of the circuit is the most important parameter. Due to this reason, we have to reduce the size of the external components, especially the inductor and the Schottky diode. We have already measured the amplifier with a 2.2µH inductor and we haven't seen any problems in terms of SPL (output voltage) and THD. Could I get additional information on the following points:
- Do you have any recommended inductor or Schottky diode with respect to a very small volume of the components (especially the height of the component)
- Do you see a risk in the stability of the boost converst in case we use a 2.2 µH inductor?
- Do you have already experience with different external components?
Thank you very much for your help
Best regards
Markus