This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV320ADC3101: The DC offset as specification.

Part Number: TLV320ADC3101

The DC offset as specification.

 

Hello,

 

Regarding to the DC offset on TLV320ADC3101, my customer is asking some question.

I know that this device has some dc offset on input block and this value is not constant each device.

The dither control register (Page 1 / Register 26) is used to reduce offset.

 

(Question)

(1) Can this offset be characterization as specification?

 (Like a generally ADC offset error on data sheet.)

If possible could you please tell me?

 

(2)Is the mechanism of this offset same as generally ADC offset error?

Or is there the relation of internal common mode voltage in the input block.?

 

Regards,

Tao2199

  • Hi, Tao,

    Please refer to below.

    • [Q1] This spec can not be characterized as it varies depending between each device and end-application.
    • [Q2] This variation is related to the general ADC behavior. Dither control register is generally used to reduce the offset, also, digital filters are available to configure a HP filter if required.

    Best Regards,

      -Diego Meléndez López
       Audio Applications Engineer