Hi,
Question 1: Are the two output power supplies (PVDD_AB and PVDD_CD) completely independent? For example, can I use two different voltages (say, I want AB with 35V for the woofer and CD at 30V for the mid/tweeter that has lower power capability)?
Corollary: are the three pins for each of the above two (three pins for PVDD_AB and three pins for PVDD_CD) also independent? For example, can I connect three power supplies of the same voltage, one to each pin, to add the power capabilities of the power supplies?
Question 2: What are the recommended types of decoupling capacitors? I'm highly reluctant to use X7R (due to microphony) in audio applications --- even for power supply decoupling. However, the NP0 caps only get to 0.1uF in 1206 size (which still fits, but it's a bit uncomfortable to place). I'm inclined to believe that it is better to place 0.01uF NP0 rather than 0.1uF or 1uF X7R --- what do you think? For the output stage (the PVDDs), would it be better a combo of 0.01uF NP0 next to the pin and a 1 or 2 or 10uF tantalum, say, 1cm away from the chip?
For the input side (the DVDD, AVDD, GVDD_xx, VBG pins), I'm inclined to think that 0.01uF NP0 is ok --- what do you think?
Notice that the assumption is: for decoupling capacitors, surface mount is better (avoid making an extra hole on the ground planes), and smaller size is better (thus, placeable very close to the pin).
What's your advice?
Thanks,
Carlos
--