Part Number: TLV320AIC3212
Customer is considering mic array solution for TLV320AIC3212 below.
Please let me know about below points.
①I think that TDM connection from the Host is below, is it correct?
⇒MCK1(G1 pin), BIN1(J1 pin: Serial Data In), BCLK1(H1 pin: TDM Clock), DOUT1(H2 pin: Serial Data Out), WCLK1(J2 pin:Frame_Sync)
②Is TLV320AIC3212 not need external X-tal? (This device is only need MCLK input by MCU.)
③About application note slau360;
On the Table 2-2, Is GPIO2's Digital Mic Ckock equal to PDM clock?
If PDM clock correct, can mic data receive below timing?
⇒Clock rise: PDM-L, and clock fall:PDM-R

④Can Mic data(×8) send to MCU by TDM below image?
WCLK1,BCLK1,DIN,DOUT -----------<TDM Bus>-------------- MCU(Mic data ×8)
GPIO2---------------------------<PDM Clock>-----------MEMS Mic(1~8)
MCLK2---------------------------<PDM Data>-------------MEMS Mic(1~2)
DIN2----------------------------<PDM Data>-------------MEMS Mic(3~4)
GPIO1---------------------------<PDM Data>-------------MEMS Mic(5~6)
GPI1----------------------------<PDM Data>-------------MEMS Mic(7~8)
⑤If unnecessary the charge pump function, are pins involved in charge pump left open or GND, OK?
Best regards,
Satoshi