Hi,
I've successfully done my preliminary design of a stereo BTL amplifier (following Figure 25 from the datasheet).
Now, I have several questions on the issue of the output filter (the inductors, specifically).
- I'm quite shocked to see the EVM use inductors with ferromagnetic core --- this is directly on the audio path, and I would assume that the non-linearity of these types of inductors is unacceptable. Why doesn't the EVM use inductors with air core?
- Regarding the output filter configuration, I'm wondering why we need two LC low-pass filters instead of one --- see the figure below showing the two other options I see:
Option 3 is in principle equivalent to option 2, but I sort of find it scary to connect a switching output directly to the speaker terminal. BTW, in both cases (options 2 and 3), the 1nF || (10nF + 3R3) snub circuits become just one snub circuit, between the speaker terminals --- instead of one snub circuit from each speaker terminal to GND.
Any comments? Notice that even though option 3 uses two inductors, they're two half-size inductors, so it would still be better than option 1. - Location of the inductors? See figure below --- that's what the air-core inductors look like (from solen.ca/product-category/inductors):
I'm thinking placing those parallel to the plane of the PCB is bad, since the EMI will hit the PCB traces with optimal coupling (correct?). But then, if we put them next to each other with the centers aligned (as if stacked to form a cylinder), that would be pessimal, right? We would have a transformer with both ports being connected to different outputs --- that's really really bad, correct?
Any suggestions? - Lastly --- has anyone considered doing the inductor in the PCB? It may be a bit too bulky, but maybe something as low as 2uH or 3uH may not be too bad; the datasheet talks about audio bandwith up to 100kHz for HD audio; with 2uH the cutoff frequency goes up to a few hundred kHz --- does this sound reasonable?
Thanks for any comments / advice.
Carlos
--