Hi there,
I set up smart Amp evaluation TAS5766MRMTEVM board connected to Pure path Mother board PUREPATH-CMBEVM and to my computer via USB connection. From the PPC-3 GUI, i could set the EQ to optimize my loud speaker performance. If I play a test signal from PPC-3 GUI application, I have a flat frequency response out of my loud speakers. If I play the test signal from other applications on my computer, the loudspeakers produce the sound, but the EQ compensation is not included, therefore the frequency response is not flat.
I would like to know how I can load the EQ settings onto the board? Does the PUREPATH-CMBEVM and TAS5766MRMTEVM combination allow me to do that?
If any additional board is needed, would you please let me know which one?
Does TI have a board where I can load the EQ settings onto and the tuning will stay on board, meaning the board can be boot by itself with the tuning on?
I saw a mention of self boot capability on the schematic of mother board but no other reference or documentation about this feature. Would you please comment on this feature.
Thanks,
Lan Nguyen