Other Parts Discussed in Thread: TPA3251, TPA3255
After completing a 2x80W power amp design, I'm having difficulty with the way TPA 3251 sounds. This is after numerous listening tests and comparisons with a 2x100W power amplifier (with good review by magazine), a 2x50W analog power amplifier and a 2x12W low power analog amplifier (powered by a Laptop 19V power supply). It is the first time I use this chip for a customer and I'm looking for ways to improve the way it sounds. The deficiency is in the mid and low end frequencies.
I'm using a pair of $1500 KEF 50th anniversary Model loudspeakers. Playing classical and soft jazz music with no EQing. My listening room is small like 20'x20'. The bass and mid-range sounded thin, lacks deep bass punch, warmness and fullness, with OK transparency. It is so obvious even a non-audiophile person can detect the big difference. The frequency response of the amp built with TPA3251 is good, -0.5dB/20HZ and -0.8dB/20KHZ with 8 ohm load.
A question came up after studying the schematic of TPA3251D2EVM, I am wondering if applying post filter negative feedback would solve my problem ? Has TI ever tested the EV board with R47,49,50,51;C73,74,75,76, and R4,12,44, and R46 all inserted ? What values are they and how do they affect the overall gain of the amplifier ? Thank you !
Engne Tang
VAC-com, Inc.