Hi Team,
The datasheet shows the following about short-circuit protection.
(page.21)
9.3.3 Short-Circuit Auto-Recovery
When a short-circuit event happens, the TPA2026D2 goes to low duty cycle mode and tries to reactivate itself
every 110 μs. This auto-recovery continues until the short-circuit event stops. This feature can protect the device
without affecting the device's long-term reliability. FAULT bit (register 1, bit 3) still requires a write to clear.
How much current does TPA2026 detect as short-circuit?
Best Regards,
Yaita / Japan disty