Part Number: PCM1690-Q1
Other Parts Discussed in Thread: ADS1672
I am developing a new product that uses an ADS1672 ADC on the input. For the output I am using a PCM1690-Q1 DAC. I was reviewing my design when it hit me that the input ADC converts the incoming signal using a 2s compliment value for input signals that are negative. I then scoured the data sheet for the PCM1690-Q1 uses the same data format but there is nothing in the datasheet that depicts the format of the digital input. I would hate to just assume that the digital output format of the ADC and DAC are the same and find out that the system doesn't work. How do I find out what the digital data format should look like and I don't mean the serial communications. Any and all help appreciated.
Regards,
Mike Lacroix