Other Parts Discussed in Thread: SRC4192,
Hi Sirs,
I am programming the AIC3268 as an I2S to Right Justified format converter for my customer. The input and output formats are:
MCLK = 24.576MHz
1. ASI1 (Input, Slave mode) -> BCLK = 1.512MHz, LRCK = 48kHz, 16bit I2S
2. ASI2 (Output, Master mode) -> BCLK = 1.512MHz, LRCK = 48kHz, 16bit RAJ
I am trying to configure the AIC3268 with the following configurations, however, I can get valid BCLK and LRCK output on ASI2, not the Audio Precision culd not decode te data. Would you pls advise if there is missing or mistake with my CodecControl configuration?
PPS configuration:
CC configuration:
Thank you and Best regards,
Wayne Chen
05/18/2017