Part Number: PCM1861EVM
Other Parts Discussed in Thread: PCM1861, PCM1863, PCM9211
Tool/software: Starterware
Hello,
I use the PCM1861EVM with the USB-I2X board. The USB-I2X board is connected to the PC via USB. When the EVM is powered up, a sample sound is transferred via USB and can be heared on the PC.
1. How can I disable the sample sound? I just want to connect a mic to the PCM1861 and hear the sound on the pc side.
2. The jumper settings for mode 0 and mode 2 are exactly the same (j8 and j11 installed, j10 removed). I just need the usb mode without SPDIF. How can I achieve this?
3. Is it possible to replace the PCM1861 with the PCM1863 on the EVM? Or do we need another EVM?
Thanks in advance
Marc