Other Parts Discussed in Thread: TPA3118D2
Hi, I would like to interface PCM 5122 with TPA3118D2. The datasheet of PCM5122 states that the outputs are gnd centered so no DC block cap is needed. On the other hand, the datasheet of TPA3118D2 states the inputs are biased to 3Vdc, in this case, do I still need a DC block cap to block the DC from TPA3118D2? If the cap is not needed, how to interface the single-ended outputs of PCM5122 to the differential inputs of TPA3118D2? Thanks in advance.