This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS5731M: Configuration

Part Number: TAS5731M

Hi,

I’m Antonio. I contact you because I am developing a new device with TAS5731M. I have some doubts that I would like to consult you because despite the arrival of I2S signals at TAs5731M, I can not seem to hear anything from the signals.

I have the next signals in TAS5731M:

Pin 19 (PDN) and 25 (RESET) --> HIGH (3.3V)

I2S

Pin 20 (LRCLK) --> Signal of 44.1 KHz

Pin 21 (SCLK) --> Signal of 2.82 MHz

Pin 22 (SDIN) --> Auidio signal

Pin 15 (MCLK) --> Signal of 12 MHz 

Question 1: 
Can the MCLK frequency be any of the limits that the datasheet marks or depends on the LRCLK signals?

The 0x00 register has value in my device 0x6C. MCLK frecuency = 256* fs = 256*44.1KHz = 12.29MHZ
       Can MCLK signal be 12MHz instead of 12.29MHz for our case?

Question 2:

I set up the following registers

0x05 --> Value 0x00 (Normal operation. Exit all-channel shutdown)

0x07, 0x08, 0x09, 0x0A --> Value 0x00 (24dB).

       The 0x02 has 0x00 value (No errors) and 0x04 register 0x05 value (I2S 24 bits).
       The remaining registers are left with the default values ​​since we do not want to perform any signal processing.
Would there be any other record that I should fit for the TAS5731M to work correctly? 

Question 3:

What is the bank switch register (0x05) ? What is it for? I
I do not know if it is mandatory to change the default value according to the frequency fs (in my case 44.1 Khz) or it is just a record for signal processing.

I await your response to continue development.

Thank you very much in advance.

Antonio Guzman