This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Need help with the TAS5615

Other Parts Discussed in Thread: TAS5615, TAS5630PHD2EVM

Hi everybody,
I am trying to design a prototype with the TAS5615 amplifier following the evaluation board but, I don't know what I have done wrong, because the amplifier get damage after 5-6 times I turn off the reset.
I attached the schematich of the board and the layout of the 2 sided PCB.
-I use a load of 11ohm which needs 100W. Please, confirm me that I can use it with this amplifier, maybe the reason of my problems is the load.
-PBTL configuration
-The input signal is a PWM generated with a microcontroller
-Power supply is the LTC3862EFE-1 from Linear, configured to obtain 45V, 4A. (Another possible reason of the failure)
The starting secuence I use is:
-Turn on the 45V power supply, but this supply don't feed the amplifier yet (there is a relay)
-Turn on the 12V and the relay (now the amplifier have both powers)
-Turn on the input signal
-Turn off the reset
The amplifier sounds, but after 5-6 times to turn on-turn off the reset, the SD pin is permanently on, and one of the outputs makes a shortcircuit with GND.

Thank you in advance for the help

TAS5615.rar
  • Hi, Lorena,

    Try turning off the reset and then slowly applying the input signal. Do not jam a huge peak-to-peak signal into the inputs, especially while the amp is starting up. Slowly increase the amplitude, and I think your failures should go away.

    -d2

  • Hi Lorena,

     

    The TAS5615 has analog input. May be your microcontroller generated PWM input signal cause the damage.

     

    Best regards.

  • Hi Attila,

    The output of the microcontroller enter in an opamp that converts the signal in a differential one, so (I suppose), after that it is also an analog signal.

    Best regards,

  • Hi Don,

    I turn off the reset without applying the input signal and the amp was damaged. Instead of turning on the ready led, it was the SD led. No variations in the power supply were detected.

    Regards,

  • Hi Lorena,

     

    The opamp will convert the input PWM signal to differential output signals. If the PWM frequency is sufficiently high the gain of the opamp would be decrease (at that frequency). In this case the output signals will be nearly analog and the high frequency PWM signal won't appear on the output signal. Maybe a few nF capacitor in parallel with the feedback resistor of the differential amplifier could set a lower cut-off frequency.

    Anyway, what is the frequency of the PWM signal?

    I hope I could help a bit.

    :)

     

    Best regards.

  • Hi Attila,

    The maximum generates frequency is 90kHz (if I remember well).  But, the latest tests that I had done were with a signal generated by the PC, with the headphones output. But, even with this, the amp was damaged before I had applied the input signal.

    Every idea is good to find the error. Thank you :)

    Regards

  • Lorena, I have reviewed your schematic and PCB layout and thought about what you have said before.  If I have understood you correctly, the following is true.

    - The TAS5615 is damaged when you take it out of RESET (that is, setting the /RESET line high).  This happens whether you are applying input signal or not.

    Is that correct?

    I will try to comment on your schematic and PCB layout, because the answer may be there.

    - SCHEMATIC:  I think you have tried to copy the TI EVM schematic.  The resolution in the schematic you sent us is not good, so I cannot be sure, but it seems so.

    I cannot tell what components you are using, because I do not have a BOM.  I am most concerned about all of the PVDD decoupling caps and the LC filter components, especially the inductors and 680nF caps.  Can you provide a BOM with data sheets for these components?

    (I think the inductors may be a problem, because they appear rather small.  This suggests they may saturate and lose much of their inductance even during startup.  I think the 680nF caps may be a problem, because they appear to be 0805 or 0603 ceramics.  Caps like that do not meet the specifications of the metal film caps we use in our EVMs, and they are not so likely to behave well in the LC filter.)

    - PCB LAYOUT:  The layout does not implement many of the important features of our EVM PCB layout.  These are shown in the EVM, of course, but they are also described in the section of the data sheet called "PRINTED CIRCUIT BOARD RECOMMENDATION" on pages 24-26 of SLAS595B.

    The most troubling item might be that it seems there is no ground to the heatsink for TAS5615.  Maybe it is there and I cannot see it.  It is vital to ground the heatsink to help control substrate currents.

    The ground plane is not wired to the device or the 2.2uF decoupling caps as strongly as in the EVM.  The EVM puts an array of vias under the device, including several directly at the PGND pins, to tie the local grounds of the device very strongly to the ground plane.  The EVM also puts 4 vias directly at the ground terminals of the 2.2uF caps to tie them strongly to the ground plane.  This layout creates very low ground impedance at the device to minimize output and power supply switching transients that could otherwise could damage it.  Your layout does not have grounding that is nearly as strong.

    I hope this can help you correct the problem you're facing.

    Best regards,

    Steve.

  • Hi Steve,

    yes, I had tried to follow the EVM. I send again the schematic, just in case you are interested. And yes, you described in a sentence what happen to me.

    SCHEMATIC: attached are the two datasheets. The inductor is one of Pulse (15uH, 5A) and the capacitor is a ceramic one (1210 size, 100V). Maybe you are right about the cap. I will try to buy a metal film one and try them

    PCB LAYOUT: yes, you are right that I didn´t place so much vias than in the EVM, And I forgot to connect the heatsink to GND. I think I can managed to connect it, but I am not sure if I can tie stronger the ground plane without send the PCB to fabrication again.

    Please, confirm me that the inductor is OK. I will try to make the corrections and let you know.

    Thank you very much,

    Best Regards,

    Lorena

    TAS5615_2.rar
  • Lorena, thank you for the schematic - it is much better.  Regarding the components, I think I can tell which inductor and capacitor you mean, but please confirm part numbers for me so I am sure.

    If the cap is the 1210 680nF 100V on page 22, I do not see a big problem with it, at least for stability.  High-K capacitors generally have high sensitivity to applied voltage, and they tend to lose a significant percentage of their capacitance with voltages hear their ratings.  But I recommend using X7R material with voltage rating twice the power supply voltage, and you appear to have chosen that already.  (Stay away from Y5V - at its rated voltage it tends to lose 80% of its nominal capacitance, or maybe even more.)

    I can't be sure about the inductor, because all that is listed is the 5A "Rated Current", which is probably a thermal rating.  What's important for stability is saturation current, which is not given.  TAS5615 requires a minimum of 14uH to be able to maintain OCP.  Without that output current may rise so quickly that the OCP circuit cannot detect it soon enough to prevent damage.  Of course, inductance of a nominal 15uH inductor can fall much lower as it saturates.

    Regarding PCB layout, please first try grounding the heatsink.  This is important for limiting substrate bounce, and it may make a big difference.

    Next, you might temporarily replace the inductors with inductors from a TAS5615 EVM.  Those are good to 15A.

    Finally, it would be possible to simulate adding vias by drilling a pattern of small holes under the device and connecting through them with very fine wire.  The chip package has only 0.15mm clearance underneath, so wire diameter would have to be less than 0.15mm diameter, AWG 35 / metric 1.4 or smaller.  This could take some work but it could be done, more quickly and cheaply than modifying the layout and fabricating new assemblies.

    Best regards,

    Steve.

  • Lorena, I hope you have had success in trying the things I suggested in my last post.  I have reviewed this further, and I want to emphasize the importance of good PCB grounding.  It is critical in high-voltage, high-current circuits, and TAS5615 is one of those.

    Our EVM uses vias at the PGND and AGND+GND points to tie them directly to the ground plane.  Other vias under the chip reinforce the connection.  These are all missing in your layout.  The consequence is that ground currents generated through the AGND+GND connection during startup can disrupt the C_STARTUP voltage, toggling the output FETs on and off.  These transients can produce larger currents than normal, not under OCP control, and they can damage a FET.  But this does not happen with grounding like the EVM, because the impedance between PGNDs and AGND+GND is very low.

    Ultimately you will need to modify your layout to get the strong grounding that's required.  But maybe you can add simple wiring to simulate vias and succeed with that as an experimental step.  Please let me know how you do.

    Best regards,

    Steve.

  • Steve, I am sorry to say that all the things that you suggested doesn't work with my prototype.

    -I made few vias under the chip

    -Added the ground connection with the heatsink. In fact, I use the TAS5615 EVM heatsink, with the difference that I only could make 1 hole instead of 2.

    -Change the output inductors. The datasheet of the new one is attached.

    I turned one the power and then turn off the reset with no input signal. There was a squeak and then the SD light turn on.

    There has to be something more that I am doing wrong or maybe this amplifier is too sensitive and if the grounding is not perfectly made, gets damaged?

    Best regards,

    Lorena

  • Lorena, I think it is difficult to reproduce the grounding under the chip in the EVM, especially at the AGND+GND and PGND pins.  This grounding is important in any high voltage and current device like TAS5615.  If grounding is not very strong, the different grounds of the chip can bounce with respect to each other, and of course this can cause damage.

    I have 2 other thoughts.

    - When you say there is "no input signal", do you mean the input is disconnected, or the PWM stream is turned off?  Or do you mean the PWM stream is driving the input but there is no audio content?

    - Can you compare what you are doing to one of our EVMs?  Of course, the grounding in the EVM is what we recommend, so that would not be an issue.

    Best regards,

    Steve.

  • Hi Steve,

    About your questions,

    -When I say there's no input signal, I mean the input is disconnected.

    -I have done the same test in the EVM. Turn on the power and then turn off the reset, and the device get not damaged. No input signal is connected.

    I think I am going to redesign the PCB, but I am afraid it will not work anyway.

    Best Regards,

    Lorena

  • Lorena, I want to be sure I have understood you.  Please let me know if I am wrong in any of the following:

    - With input disconnected, you power up the EVM with the device in reset (/RESET low), then enable the device (/RESET high).

    - When you do that test with the EVM, TAS5615 is not damaged.

    - When you do that test with your PCB assembly, TAS5615 is damaged.

    I think this reflects the importance of proper grounding and PCB layout and correct components around the TAS5615.  I believe that, with good assembly, you will succeed if you simply copy the PCB layout and use the same components as in the EVM (or full equivalents).  You are very welcome to copy the EVM PCB layout - in fact, we encourage that, always.

    Best regards,

    Steve.

  • Hi Steve,

    Yes, you undestood well. OK, I will copy the EVM  and try to use the same components.

    Could you confirm me that the 680nF ceramic capacitor and the last 15uH inductor that I have choosen are valid?

    Thank you for the help. I will let you know if I redesign the PCB and it works.

    Best regards,

    Lorena

  • Lorena, I believe I have commented before on the capacitor and inductor.  At this point, with the difficulty you have had, I can recommend only copying the EVM, including its components, into your layout.  If you can confirm this works, it will be possible to try other components and make sure they function OK.  That is the way I recommend you approach this.

    Best regards,

    Steve.

  • Hi Lorena,

    I am facing similar problem like you but with TAS5630PHD2EVM. How did you overcome this issue? What was the conclusion you arrived for SD LED ON the moment you power up the device.?

    Regards,

    Veera.

  • Hi Veera,

    Finally, I copy as much as I can the EVM board (with almost the same components), and now, it works well. I turn on the power supply (reset of the amplifier on, low level) and the SD led makes a sparkle, but I think that it is because the device is in process of configuration. Then, turn off the reset (high level) and the ready led turn on. And, al last, turn on the sound (signal comming from a PC). And it sound well without damage!

    So, following the EVM board, I made it work. But, I think that it is necessary to be very carefull with the power supply. When you turn off all the system (power supply included), be sure thar the 1mF capacitors are not charged before apply power supply again. It happens to me that, when this ocurred, the devided get damaged.

    I hope this helps you to solve the problem. Good luck!

    Regards,

    Lorena

  • Hi Lorena,

    Thank you for the information.

    Regards,

    Veera.