Part Number: PCM2707
Hello,
A while ago I attempted a very crude minimal test circuit that didn't work --- it was missing decoupling capacitors and possibly some other important connections.
I tried this time something close to the circuit in Fig. 34 of the datasheet, except that it is bus powered (like Fig. 33). Schematic is attached as a PNG image (created with gEDA's gschem, then imported into PCB designer for the board layout --- a "photo-like" image export of the top view of the board is also attached --- top layer has the Vdd plane, bottom layer has the GND plane).
The thing is not recognized by the host (Ubuntu Linux --- I expect the device to appear in the Sound Settings dialog upon connecting it). Do you see any reason why it wouldn't work?
Additional info: bypass capacitors (C1 to C6) are: C1 = 4.7uF ceramic, 0805; C2 to C6 are 0.1uF ceramic 0805. CX1 and CX2 are 20pF ceramic NP0, 0805 (the crystal specifies load capacitance = 12pF --- is my calculation correct? Would 20pF be the right value for CX1 and CX2?). RX is 1M-ohm. R1 and R2 are 22-ohm (all resistors are 0805).
Should I see a square wave at 12MHz at pin 13? (I don't have an oscilloscope so I haven't tried --- I can take it to the office on Monday to check). Please feel free to suggest any other points where I should probe and what sort of signal should I expect.
Thanks,
Carlos
--