This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPA2000D1: TPA2000D1

Part Number: TPA2000D1

Hello,

I would like to adjust the gain of this amplifier to produce a louder audio output.  Pins 4 and 5 (GAIN0 and GAIN1) can be used to adjust the gain.  The datasheet says the gains can be adjusted by changing the taps on the input resistors inside the amplifier by supplying TTL logic level (assuming 2VDC to 5VDC).  Do I need to add an external resistor network to the pins, or will supplying a straight 5VDC be acceptable to adjust the gain?  Any clarification would be greatly appreciated.