Part Number: TAS5782M
Other Parts Discussed in Thread: PCM3070
Hello,
Thank you for your support.
My customer intends to use two TAS5782M (s) with MSP430G2x
for 2.1ch high-res speaker system whose input is 96kHz I2S for L, R, Subwoofer .
*Device#1 ; L/R channel Process Flow1 BTL
*Device#2 ; Sub channel Process Flow1 PBTL
Question
Customer intend to fix MSP430G2x part number ( Flash Memory size) , but how much is the code size?
(how much Bytes should be sent from MSP430?)
I have ever used PCM3070 and its .cfg file was approx.60KB maximum ( size is
changes with process flow ),but I have no idea about TAS5782M.
With My Best Regards