Other Parts Discussed in Thread: TLV320AIC3104
Hello!
I have two questions I'm hoping you guys could help me with.
I'm working on a prototype to enable eCalls to be made from vehicles. I've looked at the various eCall reference designs provided by Texas Instrument and have zeroed in on the TLV320AIC3104. Since this is only a prototype, I'm trying to use a Stereo+Cellular headset instead of the recommended two audio jacks for mic and speaker separately.
I found the slaa454.pdf document, where the following connection is recommended.
I've used this reference in addition to the information provided from the datasheet of the 320AIC3104 as well the 320AIC3104 evaluation board datasheet.
This is the final schematic I've come up with
My first question is, have I got the headset jack connections right? Do you see any possible problems there?
Second question is what to do with the unused analog inputs ? Can I leave them as they are or do I tie them to ground with a 0.47uF Capacitor as recommended? If yes, then what package size is recommended?
Thank you for your help!