Other Parts Discussed in Thread: PCM1863
Hi TI experts,
According to the Spec , when PCM1861 is in master mode, the BCK is always at 64fs. If so, does it default to generate 32bits data per channel all the time?
Thank you
Fai
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, Fai,
When the PCM1861 is configured in master mode, the device generates the bit clock with a fixed frequency of 65×Fs, and as you mention, this configuration allows a maximum 32-bit data per channel. However, the PCM1861 will send 24 bits of data with this configuration. Software controlled devices of this family, like the PCM1863, can be configured to send 32 bits of data per channel.
Best Regards,
-Diego Meléndez López
Audio Applications Engineer