Part Number: TPA3116D2EVM
Other Parts Discussed in Thread: TPA3116D2
Hi All
I am using a miniDSP as a DAC / crossover + PEQ into the TPA3116EVM to drive 2 speakers. I am seeing that the maximum input signal into the TPA3116EVM before the output clips is about 770mVrms sin at 1kHz. This is close to 1Vp but what is the maximum input level the TPA3116EVM likes to see? The miniDSP has a maximum output of ~2Vrms with 0dBFS sin at 1kHz.
Thanks
-Mike