Part Number: DRV603
Hi team,
I have a few questions regarding DRV603 output loading. The datasheet states maximum output current is 20mA (typ) - is this peak current? Or continuous DC?
What is the minimum resistance value required on the output of DRV603 for reliable operation if the output were shorted indefinitely and input signal drove full output?
Basically, can DRV603 continuously sink current into a current limiting resistor and what would be the minimum resistance to ensure the device does not fail, overheat and get damaged (or trip internal short circuit protection).
Thanks for the support in advance!