This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPA3111D1: TPA3111D1

Part Number: TPA3111D1

TPA3111 question.docx

 

Hello,

 

We’re working on a new audio amplifier implementation. We’ve got the development kit and have begun PCB layout using a TPA3111.  There seems to be some inconsistency in the documentation that I’d like some clarity on please.

 

In revision D from October 2010, there was a 100kΩ resistor added to the AVCC line. However, there is some ambiguity as to which pin it is connected too, or both (7 & 14).

 

Assuming our power supply slew rate is <10v/ms.

 

Below are a few snippets of the spec sheet which seem to indicate tying a 100kΩ resistor to pin 14, or pin 7, and perhaps both pins by the use of the plural “pins” when discussing AVCC.

 

Please clarify the intent.

 

Thank you very much,

Gary

 

PS: The default instructions in the "E2E thread title" box within this posting form are misleading.  The webpage forces you to enter something in this box even though the instructions indicate that it is not required if the part number has been provided above.