Other Parts Discussed in Thread: PCM1792, PCM1789, TPA3132D2, TPA6211A1
Hi All some questions,
- We have two speakers (left and right) and would like to drive these independently each at a max 10W per channel (with controllable gain) speaker impedance 4ohm can someone help with a device selection for the Audio amplifier, Class D will suffice for this application.
- The preceded Audio Chain I'm trying to decide on which DAC to drive the amplifier looking at both the PCM1789 or the PCM1792 some advice on this would also be appreciated with any link to reference designs.
- On the same system we also need an output into a 8ohm load at 5VPk-Pk which is required to be either single ended or differential (universal) with controllable gain
Many Thanks