This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS5760M: Maximum Output Power

Part Number: TAS5760M

Hi Team,

I have some question as below.

1. When customer using 2kHz sampling rate, Speaker 8 Ohm and THD+N 15%, does TAS5760 can support 15W?  (Don’t care about PBTL, BTL)

Pls see below detail system requirement for using TAS5760. 


 PVDD?

-       Normal Operating voltage range : 9V~ 16V

-       Standard test voltage : 14V (It’s for 12V automotive system)


 Max RMS power?

-       Speaker RMS power is 10W, 4 Ohm.

-       Amplifier RMS power should be over 20W at 4Ohm, THD+N 10%.

-       But additional special requirement is 15W, 8Ohm at THD 15% for amplifier output.

-       Current capability should be over then 7A.

 

THD+N @ 1W sine?

-       THD+N should be below 0.1%  at 1W, 1kHz sine.

 

THD+N @ max RMS power?

-       Amplifier RMS power should be over 20W at 4Ohm, THD+N 10%.

-       When the speaker impedance is 8Ohm, amplifier continuous power requirement is 15W at THD 15%.

 

Frequency response?

-       Signal band width is 20 ~ 6000Hz

 

Idle noise?

-       There is no specific requirement.

-       SNR  : min 90dB

 

Thermal budget?

-       It depends on the Amplifier characteristic. There is no requirement on thermal budget.

 

Impedance requirement.

-       Handling impedance range : 4~8 Ohm, 4ohm impedance shall be ensured.

2. In case of BTL Mode,

  • When PVDD= 12V, Rspk = 4Ohm, THD+N = 10%, what is Power ?

  • When PVDD= 12V, Rspk = 8Ohm, THD+N = 10%, what is Power ?

  • When PVDD= 12V, Rspk = 8Ohm, THD+N = 15%, what is Power ?

 

  • When PVDD= 15V, Rspk = 4Ohm, THD+N = 10%, what is Power ?

  • When PVDD= 15V, Rspk = 8Ohm, THD+N = 10%, what is Power ?

  • When PVDD= 15V, Rspk = 8Ohm, THD+N = 15%, what is Power ?

3. In case of PBTL Mode,

  • When PVDD= 12V, Rspk = 4Ohm, THD+N = 10%, what is Power ?

  • When PVDD= 12V, Rspk = 8Ohm, THD+N = 10%, what is Power ?

  • When PVDD= 12V, Rspk = 8Ohm, THD+N = 15%, what is Power ?

 

  • When PVDD= 15V, Rspk = 4Ohm, THD+N = 10%, what is Power ?

  • When PVDD= 15V, Rspk = 8Ohm, THD+N = 10%, what is Power ?

  • When PVDD= 15V, Rspk = 8Ohm, THD+N = 15%, what is Power ?


If you have any question, pls feel free let me know.

Anthony Kim