Part Number: TAS5756M
Hello Audio Folks, a customer met a strange issue on the biqual filter for the high frequency output. The left channel is OK, but right channel is failed.
Below is the setting and result in PPC2.
Below is the frequency scan with AP using TAS5756 EVM board from TI.
The left and right channel are identical up to 5KHz, then start deviating. Left chanel follow the setting as in PPC2. Right channel seem to be no effect or something wrong there.
For TAS5754/56 and PPC2, there are no separation on the left and right channel for the biqual filter. Why left and right channel are difference. Will it be a bug in PPC2 coding?
Regards,
Kes