Part Number: TPA3106D1
What are the current requirements of the TPA3106? Looking at the datasheet, it seems like a 3A source might be sufficient, maybe even 2A.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPA3106D1
What are the current requirements of the TPA3106? Looking at the datasheet, it seems like a 3A source might be sufficient, maybe even 2A.
Hi Shawn
My application:
gain: 36 dB
supply: 26 V
load: 8 ohm
by fig 19, i guess my efficiency is about 85%, by looking at 39 W position. But not really sure if 39 W is correct position to look at.
so, by fig 20, i guess my current is about 1.5 A, which does not sound correct to me.
what difference between power consumption and power current?
(D1, by the way, not D2 :)