Other Parts Discussed in Thread: TAS5731
Hello,
Actually I am working with TAS5731M in BTL mode, and when the sound is too high the outputs are deactivated (muted).
I implemented this on a board and it worked well, but now on the new design I have this problem.
I took the same schematic (same as EVM board) and routing file for the two designs, the only thing that's changed is the thickness of the PCB (1mm to 0.8mm now).
I am reading some register before and after the TAS is muted :
- Error Status Register : Before muting, the bit clip indicator appears (0x04).
- System control Register : When the TAS is muted the value in this register change from 0x00 to 0x40. It means the outputs are hard muted but I don't know why the TAS is doing that
To restart the TAS I have to power it down and restart it.
Please find below the schematic used.
Thanks for your help
Mallyck