Other Parts Discussed in Thread: PCM1782, TPA701, TPA6205A1, TAS5342
Hi,
I like to drive a mini speaker (0.3 W nominal, 0.5 W maximal, 8 ohm) after the PCM1782 (mono). It's my first audio application and I am not sure which amplifier I should use. AB-class or D-class?
TPA701, TPA2031, TPA2036 or another one?
I have a single 5V power supply for USB-Bus and audio. The ground plane is also used for a 32-Bit MCU with DDR2-RAM. Should I build an ground island and connect it on an single point through an ferrite bend?
My application is not portable!
Regards,
Pascal