Part Number: TAS5751M
Tool/software: Linux
In my platform, cpu connect to tas5751m with i2s (4lines) port.
My platform audio config as follow:
1.MCLK=12.288M,Bclk=3.072M,LRclk=48k
2.word size is 16bit Left-Justified
Q1.when play music, we got waveform on i2s data pins,but can't hear in speaker.which register need modify?
Attach file is the tas5751m register dump of my platform.
Q2:when play music,the current of the platform raise from 400mA to 3A, and keep high during music playing.
Is the power of amplifiter config too high? Which register should be configed to draw down the current.
Thanks.