This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
For parts with date code 61QH1 and 61EG4, we observed THD+N @ 10kHz that is higher than previous lots from the past 15 years. All of the 1201 parts used from a 2.5K reel of date code 61QH1 had to be replaced.
Previously our measured THD+N with a 10kHz / 19dBu sine wave input was -108dB to -110dB. For the same measurement, this lot shows a value of -104dB typically.
The load on the output is 3.46k ohms.
The output signal level is 13dBu / 3.46VRMS
Replacing the part with one from an older date code resolved the distortion issue.
We observed the same reading from parts that were placed by our contract manufacturer and hand-soldered in-house.
NOTE: I submitted this to the TI Customer Support Center with a Customer Information Form, but they directed me to this site. I can send this form.
Bob,
The INA137 THD+Noise specification at f=10kHz has TYPICAL value of 0.0005% (106dB - see below) BUT its magnitude may vary due to normal process variation. The variation in the distortion is primarly caused by the change in the sheet resistance (+/-15%) values as well as variation in the bandwidth of the part (+/-30%).
Hello Marek,
Thanks for the reply.
I understand that we are measuring THD+N levels close to that shown in the graph. However, it seems that something must have changed in the fabrication of these parts. They have been very consistent for 12 years, but the most recent batches are showing this issue.
Was there a fabrication change?
Has anyone else reported this?
Have counterfeit versions of these parts hit the market?
Regards,
Bob Bauman
Marek,
Thanks for the update. Please let me know what you find.
We have parts that we would like to return if justified.
Bob
Bob,
This issue aligns timewise with a noise problem found at our fab. This has since been resolved but material that was fabricated in this time period is susceptible to THD+Noise issue. However, the engineer I am working with told me the lot trace code (LTC) you provided is incomplete. If we can get the full LTC, we can pin point the exact fabrication date and based on the assembly date we can extract from the LTC, we will be able to conclusively determine whether the wafer lots in question were effected.
Bob,
The process engineer has confirmed that the lot in question was produced AFTER the process change was implemented, which means that the temporary issue we had with the process does not explain your problem and therefore, the fix will NOT eliminate a possibility of the "issue" to show in the future lots.
Having said that, you wrote before:
“Previously our measured THD+N with a 10kHz / 19dBu sine wave input was -108dB to -110dB. For the same measurement, this lot shows a value of -104dB typically.”
So you actually used to see THD+Noise at 10kHz slightly better by few dB's than datasheet curve below shows (0.0005% ~ -106dB) and now you see it 2dB lower. As I said before, these are typical specs that may somewhat vary over process variation. But seeing that your issue occurs at 10kHz, which is right at the inflection point of the THD+Noise curve, any variation in load or bandwidth (may vary up to +/-30%) could easily produce such effect.