Part Number: TLV320AIC3206
Hi
The analog input to TLV320AIC should be AC-couplied to allow the common mode voltage within the device spec.
According to the datasheet, the analog input range as absolute maximum ratings is AVss to AVdd + 0.3.
So, even if the input is AC-coupled, the input must be over AVss, is it correct?
Now we assume AVss=0V and the input is 2Vpp (+1V, -1V, 0V center) after AC-coupled.
How does the user bias to analog input with the analog input specification (AVss to AVdd + 0.3)?
What is the "CM" in Audio input max ac signal swing on datasheet?
BestRegards