Part Number: PCM5142
My customer want to use PCM5142 for new design.
But would you please have your opinion?
Q1) 4 wire I2S input as "SCK=BCK" is OK for auto-configure the clock tree and PLL ?
So, Table 32 on Data Sheet page47 discribes the relationship between SCK and Sampling frequency (LRCK),
but Customer will use as following case a),b) as SCK=BCK.
Customer says it works correctly in PCM5142 EVM without PLL setting, but customer want to have your confirmation.
a)LRCK=352.80KHz SCK=BCK=22.5792MHz
b)LRCK=384.00KHz SCK=BCK=24.5760MHz
Q2) LRCK 256KHz 4-wire mode on SCK=BCK=16.384MHz can be auto-configured?
This setting seems such as " Not Common audio sample frequencies" and concern is customer must set PLL setting....
Do you think 4-wire auto-configure the clock tree and PLL available for LRCK=256KHz and SCK=BCK=16.384MHz?
Customer says PCM5142 EVM works correctly with auto-configured in case LRCK=256KHz/SCK=BCK=16.384MHz.
How do you think? ( Its OK because multiple of 32KHz ?)
Best Regards