Part Number: TAS5753MD
Hi Team,
Customer uses the TAS5753 on the monitor application. Currently there are no obviously abnormal found on this project.
Do you have any concern if customer use the following values?
1.HPVDD/AVDD Pin14/19,dstahset suggest 4.7uf+0.1uf. customer uses 10uf+1uf
2.OSC-RES pin 22 recommended 18K to GND,customer uses 18.2K
3.DVDD_REG pin24 datasheet suggest to use. 4.7uf+0.1uf ,customer uses4.7uf,
4. BST&Out pin ,suggest to use 0.01uf ,customer uses 0.033uf
What is the side effect if using the customer select values?
Thanks,
SHH