This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS6424-Q1: 96KHz optical input in PPC3

Part Number: TAS6424-Q1
Other Parts Discussed in Thread: TAS6422-Q1

Hello

Customer want to evaluate TAS6424-Q1 or TAS6422-Q1 for a candidate of FY2018 model.

Please advise .

 

Q1 96kHz input

I can operate TAS6424-Q1EVM at fs=48KHz in PPC3.

Please let me know the way to input 96KHz( Optical) in PPC3.

In the EVM user's guide SLOU453 says;   " If sampling frequency is greater than 48 kHz, select 96 kHz from the “Input FS” pull down."..

Where is Input FS button?

Q2 volume Gang

The volume in TAS6424-Q1 ( also TAS6422-Q1 ) can not be ganged?

It seems no gang function in PPC3.

Best Regards