Hi,
I would like to ask a question for PCM1808 ADC.
Would it be a problem if there is continous LRCK and BCK input to PCM1808 (from DSP) when the device VDD/VCC are OFF?
We observed that when there are no VCC or VDD to the PCM1808, but the LRCK or BCK signals keep HIGH from DSP, it will rise the VDD of PCM1808 to around 2.2V.
Looking forward for your favourable response.
Thanks