Other Parts Discussed in Thread: PCM1681, , PCM1608
I have a customer situation that has popped up (bad pun) and could use an assist. The system uses a PCM1608 and the DRV632; and we are having issues with a ‘pop’ when power is removed unceremoniously; not common but still possible in our system. Basically the PCM1681 DAC generates a pop because the output is biased to mid-rail; this is common to most DACs I think. The DRV632 copes with this if it is muted but does pass a pop through as the rail collapses.
So we do have a voltage monitor on the supply line for the DRV32; it has a #FLAG open drain output that senses the battery voltage collapse and triggers the #MUTE on the DRV632; but this is ineffective if the DRV632 rail also collapses. Does the UVP function operate differently than the MUTE function as it relates to a low voltage/shutdown operation on the DRV632? The datasheet isn’t super clear as to whether this UVP function is there for eliminating pops, limiting current in a low VDD situation, or anything.
Any ideas welcome!