Performing thermal testing of a 2-channel audio amplifier based on TAS5613A in PHD package I encountered a problem of failures of the external protection Schottky diodes on the chip outputs.
Amplifier Configuration
The amplifier schematic is similar to the TAS5613PHD2EVM evaluation board schematic with two channels in BTL mode powered from 36V 300W SMPS. The amplifier has been designed to work with 4Ω nominal loads.
Each of the four TAS5613A half-bridge outputs OUT_x has two Schottky diodes with reverse polarisation connected. One between the output and the board ground and the other between the output and the chip PVDD supply rail. The diodes used are MBRS360T3G (SMC package) from ON Semiconductor.
The two amplifier outputs drive two step-up transformers loaded with two 50Ω resistive loads. The transformer primary windings are connected to the amplifier outputs trough coupling capacitors (2 x 1000µF in series). The amplifier board, the SMPS and the two transformers with coupling capacitors are placed in a fully enclosed metal enclosure (19” rack type).
The Test
In order to estimate the enclosure internal temperatures corresponding to the chip two over-temperature alarm thresholds (100°C and 125°C) the amplifier was driven from continuous 1kHz sinusoidal source so it would produce 71W on each of the two resistive loads. Accounting for the transformers and coupling capacitors efficiencies this corresponds to around 82W (18.5VRMS, 4.44ARMS) per each of the chip two BTL outputs (164W total).
The Failure
The alarm output corresponding to the TAS5613A junction temperature of 100°C was activated at around 57°C air temperature inside the enclosure and the amplifier continued to work as expected. Just before or right after the second alarm output corresponding to the chip 125°C junction temperature was activated one or two of the protection Schottky diodes failed (they went short circuit). At that point, the temperature in the amplifier enclosure reached around 62°C.
The diodes are mounted on the board bottom side, hence they are located in the small area between the enclosure bottom and the board (around 5mm gap).
It seems the diodes failed due to their thermal inability to dissipate the required power at such temperature.
The Problem
How to estimate the power each of the eight Schottky diodes needs to dissipate assuming in a practical implementation a user could drive the amplifier continuously to its maximum power limited only by what the power supply can provide?
Situation may be more complicated if saturation of the output transformers at low frequencies is possible (i.e. no high-pass filters on the amplifier inputs).