Other Parts Discussed in Thread: CC3200, , TPA2012D2
Tool/software: Starterware
Hi all,
I am new to audio applications. I am doing a VoIP application using TLV320AIC3106 I2S interfaced to CC3200, with asterisk as my VoIP server. I am trying to send audio data in RTP stream as G.711 codec. I selected TLV320AIC3106 audio codec. This is the features of G.711.
- Sampling frequency 8 kHz
- 64 kbit/s bitrate (8 kHz sampling frequency × 8 bits per sample)
I have attached the schematic of my application. Please verify whether it is correct. I am using a condenser mic with mono configuration. Is it possible to encode condenser mic out with the attached circuit to a format which can be used to encode it as G.711 using 3rd party software codec?
If I am using a 12.288MHz crystal to MCLK, Fsref would be 48KHz (no PLL) and ADC Fs can be set to 8KHz. Is it possible to read audio data of 16 bits, 8KHz sampling rate using I2S?
Thanks & regards,
Vishnu Pradeep