This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM1875: Getting lot of noise distortions when connected with 12VDC 1A supply

Part Number: LM1875
Other Parts Discussed in Thread: TPA3128D2

Hi,

I am using LM1875 20W Audio Power Amplifier IC and made a circuit as given in the datasheet for Typical Applications For Single Supply Operation, I am giving the supply of 12VDC 1A and connected speaker load of 5W 8 ohms(Speaker part no: CSS-40408N) but I am getting lot of noise distortions, can anyone kindly let me know how I can resolve this issue, as I am new to this audio amplifier.