Other Parts Discussed in Thread: TPA3136D2
Hello,we use TPA3110LD2 for design 1*25W 4ohms,in my design,there is have MP3 Bluetooth radio with amp board,now we face same question is that when using TPA3110L will be occur Interfere with radio,now we use CS8618 to replace TPA3110L,it will be ok,because CS8618 and TPA3110L is P2P,but now we want to TPA3110L replace CS8618,but need to solve Interfere with radio issue,beside,middle Power,now we also have used TPA3118/TPA3116 MP,TPA3118 and TPA3116 also meet the same question,could you help to give same suggestion for me to solve it,below is current Schematic for CS8618 is same to the TPA3110L,tks!