This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV320ADC3101: Generating Master Clock from BCLK

Part Number: TLV320ADC3101

Hi,

Could TLV320ADC3101 support the 3-wire PCM ?
For the audio serial interface configurations, 3-wire PCM is mentioned in the application report however it isn't mentioned whether TLV320ADC3101 can support it or not.

http://www.ti.com/lit/an/slaa469/slaa469.pdf

Best regards,
Kato

  • Hi, Kato-san,

    The TLV320ADC3101 is able to generate the required internal clocks using BCLK and the internal PLL, as depicted in the app note you are mentioning.

    Basically, BCLK should be selected as the source for the PLL, and PLL_CLK as the source for ADC_CLKIN. The dividers should be set accordingly to meet the clock specifications from the datasheet.

    Best Regards,

      -Diego Meléndez López
       Audio Applications Engineer

  • Hi Diego-san,

    Thank you for your prompt reply.
    I understood.

    Best regards,
    Kato