Hello,
we have an external 8MHZ clock which is fed into the PCM1863 at SCKI pin. PCM1863 is controlled via I2C and should operate in master mode with 48KHZ fs.
Now we need some help in the following points:
1. Calculate the PLL dividers R, J, D, P (page0, registers 0x29...0x2D)
2. Calculate the ADC and DSP1/2 CLK SRC dividers (page0, registers 0x21...0x23)
3. Calculate the PLL_SCK, SCK_BCK and SCK_LRCK dividers (page0, registers 0x25..0x27)
4. Correct startup programming sequence
Thanks in advance
Marc