Tool/software: Code Composer Studio
Our products use DAC3101, the output signal distortion is very large, to 1.86%.
A foreign recorder ZOOM H6, distortion is only 0.0012%.
I use a 44.1k sample rate 1kHz sine wave wav file, play on ZOOM H6, and use audio analyzer AP ATS-2 to test the distortion of 0.0012%. (this shows that the wav file is normal. )
Using the same wav file to play on our products, the AP ATS-2 test has a very high distortion, to 1.86%.
What's the reason, please?
Processing Block uses PRB_7, and IIR uses default parameters,
You've also tried using PRB_1, using default parameters,
As a result, the distortion is the same.
DAC3101 tuning has been tested (the right part of the picture below) no problem.
Test method is: input signals from AIN1 and AIN2, signal routing is also set, the two inputs for the signal source, and other signal source is set to disconnect, test the output signal. Distortion 0.014%.
Also check the I2S control signal, the left part of the picture below, the timing of the signal is correct, using the standard I2S mode.