Part Number: TAS5782MEVM
Hello,
I am attempting to use a TAS5782MEVM with a PPCMB (rev F), and have been unsuccessful using the analog input. I can successfully achieve an amplified output by using the USB input or the digital I2S input, however not when using the analog input.
When first configuring the device within the PurePath Console 3, I select the TAS5782 app, select the Stereo 2.0 speaker configuration, select USB In, then select Standard Processing (2.0 48k). The console configures the PPCMB and the TAS5782MEVM, and when an input is applied, an amplifier output is obtained. However, when these same steps are taken, but with an analog input, there is no output.
Are there any extra steps that need to be taken to use the analog input on the PPCMB?
Thanks,
Hanna