Other Parts Discussed in Thread: TINA-TI, , PCM1789
Tool/software: TINA-TI or Spice Models
I am trying to use the TPA6138A2 both as LPF/diff to single and as audio amplifier. I followed the datasheet exactly for 2nd order LPF and amplifier but the output sound is noisy. Then after days of not able to make it work, i tried the simulation of TPA6138A2 as provided by the TI. Herein, the model does not simulate giving me error saying:
Current of component: U2.XU5.XR108.VSENSE
Node: 132
Component/Terminals: .U1 XU5.45
My circuit is attached herewith. I have a 0.5uF capacitor before the LPF as indicated by the datasheet. Also I have 1uF at the input of the amplifier. Attached is also the schematic.
Is there any problem with the TPA6138? I don't see me doing anything wrong with the circuit.