Part Number: PCM5122EVM-U
Other Parts Discussed in Thread: PCM5122
Hi,
I just recently got the PCM5122 EVM board. I connected the board to my laptop (The driver is automatically installed). I opened some music files but I can not hear anything coming out from the left and right RCA ports. I've attached the instruction that I followed to configure the board. The line "W3 shunt all pins except 6.7, and 14" is confusing. Does it mean connect all the pin in W3 horizontally except pins 5-6, 7-8 and 13-14 or connect all the pin in W3 except for TP16, TP7 and TP14?.
In addition, can you show me how to do the configuration for the I2S inputs.
Thank you,
Thanh Tien Truong