This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM4950: LM4950

Part Number: LM4950

Hi,

I am using LM4950 audio amplifier with DAC to amplify my audio signal. The output of the LM4950 is connected to the transformer and the output of the transformer is connected to ultrasonic transducer.

The shutdown pin is continuously high, which means that the amplifier is continuously on.

I generate 10ms of chirp signals (ultrasonic range > 20kHz) which repeats after every 300ms.

When I play the sound, I hear some clicks from the amplifier even I am not turning on and off the amplifier. At the output of the transformer, the signal is also distorted.

Can somebody explain why am I hearing the sound and how can I remove it?

Best Regards