Part Number: TLV320AIC3107EVM-K
Other Parts Discussed in Thread: TLV320AIC3107
Hi,
I have been trying to get started with the EVM but am having trouble getting connected. I receive "Connect a USB Cable to EVM" when I launch the software. I have verified the position of the jumpers and switches on both boards (although I didn't see any indication of what to do with the SW1 and SW3 of USB board). I then followed the steps to revive a USB Audio EVM (e2e.ti.com/.../2790.how-to-revive-a-usb-audio-evm).
Currently diodes D2-5, and D7, D8 are lit when connected (D6 is not lit) and Windows (Win10) recognizes the EVM as two Audio inputs/output in device manager. The driver is provided by Microsoft (version 10.0.14393.0), and will not install drivers from NI-VISA or those provided by TI over these.
I'm not sure what to do if windows recognizes the device, the device itself is reading connected, but the EVM software won't connect. Any help will be greatly appreciated.
Thanks,
Steve